AXIS#.VL.ARPF1 TO AXIS#.VL.ARPF4

Description

AXIS#.VL.ARPF1 sets the natural frequency of the pole (denominator) of AR filter 1. This value is FP in the approximate transfer function of the filter:

ARx(s) = [s²/(2πFZ)² +s/(QZ2πFZ) + 1]/ [s²/(2πFP)² +s/(QP2πFP) + 1]

 

The following block diagram describes the AR filter function; note that AR1 and AR2 are in the forward path, while AR3 and AR4 are applied to feedback:

AR1, AR2, AR3, and AR4 are used in velocity and position mode, but are disabled in torque mode.

Discrete time transfer function (applies to all AR filters)

The velocity loop compensation is actually implemented as a digital discrete time system function on the DSP. The continuous time transfer function is converted to the discrete time domain by a backward Euler mapping:

s ≈ (1-z-1)/t, where t = 62.5 µs

The poles are prewarped to FP and the zeros are prewarped to FZ.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Hz

Range

5 to 5,000 Hz

Default Value

AXIS#.VL.ARPF1: 675 Hz

VLARPF2 to VLARPF4: 500 Hz

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.ARPF1

5011h

10h

Unsigned32

-

1000:1

Read/Write

No

AXIS1.VL.ARPF2

5011h

11h

Unsigned32

-

1000:1

Read/Write

No

AXIS1.VL.ARPF3

5011h

12h

Unsigned32

-

1000:1

Read/Write

No

AXIS1.VL.ARPF4

5011h

13h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6000

1

6000 (0x1770)

AXIS1.VL.ARPF1

Signed32

Read/Write

Yes

71536

2

6000 (0x1770)

AXIS2.VL.ARPF1

Signed32

Read/Write

Yes

6001

1

6001 (0x1771)

AXIS1.VL.ARPF2

Signed32

Read/Write

Yes

71537

2

6001 (0x1771)

AXIS2.VL.ARPF2

Signed32

Read/Write

Yes

6002

1

6002 (0x1772)

AXIS1.VL.ARPF3

Signed32

Read/Write

Yes

71538

2

6002 (0x1772)

AXIS2.VL.ARPF3

Signed32

Read/Write

Yes

6003

1

6003 (0x1773)

AXIS1.VL.ARPF4

Signed32

Read/Write

Yes

71539

2

6003 (0x1773)

AXIS2.VL.ARPF4

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.VL.ARPF1

6000

Float

Read/Write

-

AXIS1.VL.ARPF2

6001

Float

Read/Write

-

AXIS1.VL.ARPF3

6002

Float

Read/Write

-

AXIS1.VL.ARPF4

6003

Float

Read/Write

-